Skip to main content

availableEvent

Description

Check if there is a valid received packet. However, this only works after receiving the release event packet (data: 0). That is, it checks whether the ROBOTIS Remote Controller button is released and then pressed again.

Syntax

  • availableEvent()

Parameters

  • None

Returns

  • True(1) if valid data is received.
  • False(0) otherwise.

Example

RobotisRemoteController rc100(Serial1);
Serial.begin(115200);
rc100.begin();

if(rc100.availableEvent()) {
Serial.println(rc100.readEvent());
}