Skip to main content

CM-100 Task Code Download Guide

Preparation

  1. Please open a task code file(*.tsk) to download from RoboPlus Task.
  • You can open it by double-clicking.
  • You can open it by using the open a file function of RoboPlus Task.
  • You can open it with drag & drop in the RoboPlus task.
  1. Connect the controller([CM-100]) with your PC by using a [USB Downloader(LN-101)].
  2. Connect 2 double AA batteries then turn the power for the controller (CM-100) on.

img_01

Download

  1. Connect the controller before downloading the task code. To download the task code, the controller must be connected to the PC. (Please refer to controller information for information on how to connect the controller to the PC.)

  2. Select the correct COM port (if you know) or else use the "Automatic Search" function to easily find out the appropriate port.

    img_02

    If RoboPlus Task is unable to find a controller, the following error message will be shown.

    img_03

  • Check if the controller is connected to the PC.
  • Check if the controller is turned on.
  • Check if the correct communication port was chosen.
  1. Select the download menu.

    img_04

    If the program has an error, you must find the error and correct it. (See rule check error messages)

  2. Download the program.

    img_05

    If the downloading fails, it will automatically try again from the beginning.

  3. Execute the task code -> Your robot will move. Turn on the controller and execute the downloaded task code.