Skip to main content

The CM-550 can be connected to the PC via Micro USB port to download task(.tsk3) and motion(.mtn3) files.

  1. Connect USB cable to PC.

  2. Connect the other side of Micro USB cable to CM-550 controller. The controller will be powered by USB and turned on automatically.

  3. Luanch R+ Task 3.0 and press the Connect icon on the bottom left corner.

  4. Select the serial port to use.

  5. Press the Connect icon.

  6. CM-550 will be connected to the PC with 3 beeps.

Pairing Bluetooth

The BLE module in CM-550 can be also paired with BT-410 Dongle to connect the PC, but wireless connection will be slower than wired connection when downloading.

  1. Turn on the CM-550.

  2. Connect BT-410 Dongle to the USB port of the PC.

  3. Bring the MODE button of CM-550 closer to the BT-410 Dongle to pair automatically.

  4. Luanch R+ Task 3.0 and press the Connect icon on the bottom left corner.

  5. Make sure to check on Use USB Dongle option when using BT-410 Dongle.

  6. Select the serial port to use.

  7. Press the Connect icon.

  8. CM-550 will be connected to the PC with 3 beeps.

info

NOTE :

  • Bring the MODE button of CM-550 closer to the BT-410 Dongle to pair automatically.
  • Once BT-410 Dongle is paired successfully, the connection will be maintained within the range of Bluetooth signal.
  • Once BT-410 Dongle is paired successfully, paired device will be automatically connected within the range of Bluetooth signal.