Skip to main content

Community Showcase
: Inspiring Projects from Our Users

The DYNAMIXEL ecosystem thrives on the creativity and innovation of our users. We are thrilled to showcase some of the remarkable open-source projects developed by talented individuals, top universities, and pioneering companies around the world. These projects demonstrate the versatile capabilities of DYNAMIXEL actuators and how they empower developers to push the boundaries of robotics.

Discover how your peers are leveraging DYNAMIXEL technology to build the future, one groundbreaking project at a time. Many of these incredible advancements are proudly Powered by DYNAMIXEL.

Humanoids & Legged Robots​

PhoneBot project image

PhoneBot

Developed by: UCLA Robotics & Mechanisms Laboratory (RoMeLa)

A humanoid platform that reuses a smartphone for sensing, computation, and interaction. Thirteen DYNAMIXEL XL430-W250-T actuators drive its legs and torso, supporting walking, visual following, and mobile telepresence.

Micro Duck Project Image

Micro Duck

Developed by: Pollen Robotics

Microduck is a 25 cm biped robot with fifteen DYNAMIXEL actuators. Its open-source software and reinforcement learning stack let users train behaviors in simulation and deploy them on the robot.

Microban project image

Microban

Developed by: Marc Duclusaud / Rhoban, University of Bordeaux

A 30 cm, 3D-printable humanoid with nineteen DYNAMIXEL XL330-M288-T actuators and a Raspberry Pi Zero 2W. Published software, mechanical designs, and assembly guides support hands-on robotics education and experimentation.

Olaf Robotics Project Image

Olaf Robot

Developed by: Walt Disney Imagineering

Disney Imagineering's physical Olaf robot, controlled with RL using animation references. It uses DYNAMIXEL XH540-V270, XH430-V210, and XC330-M181 actuators.

ToddlerBot Project Image

ToddlerBot

Developed by: Stanford University

An open-source humanoid platform for learning locomotion and manipulation. Its DYNAMIXEL-based design supports reinforcement learning, imitation learning, teleoperation, and deployment of learned whole-body behaviors.

Q8bot project image

Q8bot

Developed by: Yufeng (Eric) Wu

A palm-sized, open-source quadruped powered by eight DYNAMIXEL XL330-M077-T actuators. Its motors plug directly into a central PCB, enabling a compact, cable-free design for walking, trotting, and jumping.

D’Kitty Project Image

D’Kitty

Developed by: ROBEL Research Team

A twelve-DOF quadruped from ROBEL for learning-based locomotion research. Built with DYNAMIXEL actuators, it supports standing, orientation, walking, and sim-to-real experiments on varied terrain.

Poppy Humanoid project image

Poppy Humanoid

Developed by: Poppy Project / Inria Flowers

An open-source, 3D-printed humanoid with twenty-five DYNAMIXEL actuators. Its modular body and articulated spine support research and education in locomotion, human–robot interaction, and embodied learning.

Robotic Hands & Grippers​

MIDAS Hand Project Image

MIDAS Hand

Developed by: UCLA Robotics & Mechanisms Laboratory (RoMeLa)

An open-source anthropomorphic hand for dexterous manipulation and sensing research. Its 16-DOF architecture uses thirteen DYNAMIXEL XM335-T323-T actuators.

CRAFT Hand Project Image

CRAFT Hand

Developed by: University of Illinois Urbana-Champaign, University of California Irvine

A tendon-driven anthropomorphic hand combining rigid links and soft joints for compliant, dexterous manipulation. It uses fifteen DYNAMIXEL XL330-M288-T actuators.

House of Dextra Project Image

House of Dextra

Developed by: University of California San Diego, University of California Santa Barbara

An open-source framework that jointly optimizes robotic hand designs and control policies. Its modular hardware supports different finger counts, joint configurations, and palm shapes using DYNAMIXEL XL330-M288-T actuators.

EN02-OP Project Image

EN02-OP

Developed by: Westwood Robotics

A high-performance, open-source robotic hand designed for advanced manipulation tasks, utilizing DYNAMIXELs for precise control.

Ruka-Hand Project Image

Ruka-Hand

Developed by: New York University

An open-source, 3D-printable robotic hand designed for accessibility and research, often built with DYNAMIXEL actuators.

Orca Hand Project Image

Orca Hand

Developed by: ETH Zurich

A modular and powerful open-source robotic hand for dexterous manipulation, showcasing the capabilities of DYNAMIXELs.

LeapHand Project Image

LeapHand

Developed by: Carnegie Mellon University

A low-cost, highly capable, and open-source anthropomorphic robotic hand, often integrating DYNAMIXEL actuators.

D’Manus hand anatomy

D’Manus

Developed by: Carnegie Mellon University, Meta AI (FAIR)

An open-source, three-fingered, 10-DOF robotic hand for dexterous manipulation and robot learning. DYNAMIXEL XM430 actuators drive its joints, while ReSkin sensors on the palm and fingertips provide tactile feedback for tasks such as picking and sorting objects.

D’Claw Project Image

D’Claw

Developed by: ROBEL Research Team

A three-fingered, nine-DOF manipulation platform from ROBEL. Its DYNAMIXEL actuators support real-world reinforcement learning experiments such as turning objects, grasping, and coordinating finger motions.

OpenHand Project Image

OpenHand

Developed by: Yale University

A project focusing on open-source, customizable, and accessible robotic hand designs, with DYNAMIXELs as a common choice for actuation.

Robot Arms & Bimanual Systems​

TRLC_DK1 Project Image

TRLC-DK1

Developed by: The Robot Learning Company

An open source dev kit for AI-native robotics. The leader arm uses seven DYNAMIXEL XL330-M077-T actuators.

ALOHA Project Image

ALOHA

Developed by: Stanford University, UC Berkeley, Meta

An open-source bimanual teleoperation and imitation learning system. The original ALOHA pairs DYNAMIXEL-powered WidowX leader arms with ViperX follower arms to collect demonstrations and learn fine manipulation tasks.

MikataArm six-DOF variant designed by Yoshihiro Shibata

DYNAMIXEL MikataArm

Developed by: ROBOTIS Japan / Yoshihiro Shibata

A family of ROS-compatible robot arms for education, research, and RoboCup@Home. DYNAMIXEL X-series actuators power the joints, with published control examples for teaching motions and inverse kinematics.

EvoArm project image

EvoArm

Developed by: AliShug

A 3D-printable desktop robot arm with three DYNAMIXEL AX-12 / AX-18A actuators and a two-DOF wrist driven by XL-320 actuators. Published designs, Arduino firmware, and a Python inverse-kinematics application support DIY builds.

Poppy Ergo Jr project image

Poppy Ergo Jr

Developed by: Poppy Project / Inria Flowers

A six-DOF educational robot arm built with DYNAMIXEL XL-320 actuators, 3D-printed parts, and a Raspberry Pi. Interchangeable gripper, pen-holder, and lamp tools support introductory robotics and creative programming.

Poppy Ergo project image

Poppy Ergo

Developed by: Inria Flowers / Poppy Project

A six-DOF research arm powered by six DYNAMIXEL MX-28 actuators. Its 3D-printed structure and Python control tools support experiments in artificial curiosity, learning, and robot interaction.

Teleoperation & Demonstration Devices​

LEGATO Project Image

LEGATO

Developed by: The University of Texas at Austin, The AI Institute

A cross-embodiment imitation learning framework built around a handheld gripper. The tool collects human demonstrations and transfers learned manipulation skills to different robots.

GELLO Project Image

GELLO

Developed by: University of California Berkeley

A General, Low-Cost, and Intuitive Teleoperation Framework for Robot Manipulators

Mobile Manipulators​

LeKiwi Project Image

LeKiwi-DYNAMIXEL

Developed by: SIG Robotics team at the University of Illinois Urbana-Champaign

LeKiwi - Low-Cost Mobile Manipulator (DYNAMIXEL Edition)

Mobile ALOHA Project Image

Mobile ALOHA

Developed by: Stanford University

A mobile bimanual manipulation platform that combines ALOHA with a wheeled base and whole-body teleoperation. Its DYNAMIXEL-powered ViperX arms enable imitation learning for tasks such as cooking, cleaning, and using cabinets.

Social & Bio-inspired Robots​

Reachy-Mini Project Image

Reachy-Mini

Developed by: Pollen Robotics

Reachy-Mini is a small, agile, and versatile robot designed for research and education in robotics. It uses nine DYNAMIXEL XL330-M288-T actuators.

AquaMILR+ Project Image

AquaMILR+

Developed by: CRAB Lab

An untethered limbless robot designed for complex aquatic terrain navigation. It uses DYNAMIXEL 2XL430-W250-T and 2XC330-T288-T actuators.

Share Your Project!​

The DYNAMIXEL community is a vibrant hub of innovation. If you have an open-source project that utilizes DYNAMIXEL actuators, we'd love to hear about it and potentially feature it here!

Your Idea, Powered by DYNAMIXEL. Let's build the future together.

Contact us to share your project